This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using this ADC with a TSW14J57EVM board. And i was trying to use internal clock LMK2582. I programmed ADC EVM board with settings as:
Nyquist - 1st zone
Clock - LMK2582 to ADC
Sample rate - 1536 Msps
mode - bypass and 14 bit.
then i programmed the EVM. After which i tried changing the divider from 8 to 16 but it automatically changed itself to 32 and now i dont know what am i doing wrong can you help me with this.
Hi Pavitra,
I have noticed this most often occurs when the LMX2582 device:
To avoid this, I suggest to load a configuration file. If you want, I can create a 1536MHz output frequency configuration file using TICS Pro and then convert it into the appropriate ADC32RF45 GUI format for you. If you are interested in this, please let me know.
Thanks, Chase
Yes if you can provide GUI for this then it will be very helpful. If possible can u also add instructions to use it along with it.
Pavitra,
The GUI is called TICSPRO (www.ti.com/.../TICSPRO-SW). Choose the Select Device tab and choose PLL+VCO, then choose LMX2582. This should pull up the LMX2582 GUI. We typically use this to generate the registers for any of our clocking parts. However it is important to note that the format of the register text file is different than what the ADC32RF45EVM GUI uses, so you must reformat into the correct format. Try this configuration out. It's always possible that the one included in the ADC32RF45 folder is non-functional.
LMX2582 0x00 0x0x02 0x00 0x0x00 0x46 0x0000 0x45 0x0000 0x44 0x0089 0x40 0x0077 0x3E 0x0000 0x3D 0x0001 0x3B 0x0000 0x30 0x03FC 0x2F 0x00CF 0x2E 0x1FA3 0x2D 0x0028 0x2C 0x0000 0x2B 0x0000 0x2A 0x0000 0x29 0x03E8 0x28 0x0000 0x27 0x8204 0x26 0x002E 0x25 0x4000 0x24 0x0411 0x23 0x021F 0x22 0xC3EA 0x21 0x2A0A 0x20 0x210A 0x1F 0x0601 0x1E 0x0034 0x1D 0x0084 0x1C 0x2924 0x19 0x0000 0x18 0x0509 0x17 0x8842 0x16 0x2300 0x14 0x012C 0x13 0x0965 0x0E 0x018C 0x0D 0x4000 0x0C 0x7001 0x0B 0x0018 0x0A 0x10D8 0x09 0x0302 0x08 0x1084 0x07 0x28B2 0x04 0x1943 0x02 0x0500 0x01 0x0808 0x00 0x2218
Thanks, Chase
Sorry to not mention this beforehand but it was not like it never worked. It sometimes work fine and sometimes show the problem i mentioned above. So i dont know what is i am doing differently which is causing this error
Hi Pavitra,
I'm not sure if there is any particular reason as to why the graphical issues occur, so when this happens I suggest to just reset the GUI and powerdown the device before reconnecting, if applicable. It's good to know that it does work sometimes. Is there any pattern at all as to when it works? Such as loading a configuration file for all of the devices at once? I suggest to get the EVM in a functional state, press the Read All registers button (which may take a minute or so) and then press the Save button to save the configuration.
Thanks, Chase