Part Number: DAC37J84EVM
I try to connect the DAC37J84 EVM with the Xilinx ZCU102 to test the DAC performance. However as no sync routing to the FMC connector in this FPGA board, as it suggests from this https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1073886/dac37j84evm-xilinx-eval-boards-match-for-dac3xj8xevm/3975193?tisearch=e2e-sitesearch&keymatch=zcu102#3975193,
we should connect SYNC to a spare SMA on the Zync board that routes to spare FPGA pins and connect it to J21 pin 1 (CMOS_SYNC_AB) on the DAC EVM.
I am wondering do I need to do any modification to the code or I can use the same source code for KCU105 and DAC38RF82.
Many thanks
Rory