Part Number: ADC128D818
Dear Sir/Madam,
We are using ADC128D818 for voltage monitoring applications. To make the voltage level compatible with the ADC input range, potential dividers have been used. During measurement, we are observing about 1% reduction in the value compared to expected value. For example if 1V is expected, then actual measured value is 990mV. We would like to understand the reason for this issue. Is there any source impedance mis-match?
Regards,
Saravana