Part Number: AFE58JD28EVM
Other Parts Discussed in Thread: AFE58JD28, TSW14J50EVM
Hi
In our company, we are working on a measurement system based on several ultrasound cards (transmitters and receivers).
We are interested in replacing the cards we have (from another company) with a number of AFE58JD28 and TSW14J50 cards, when we hoped we could use the HSDCPro Automation DLL.
During the integration work, we discovered that the use of the dll requires the GUI to be open and connected directly to the board.
Here are some questions:
1) Is there a way to use the HSDCPro Automation DLL for several cards simultaneously, without having to use the UI to switch from board to board?
2) We saw that if there are pop-up messages (on the UI screen), the dll commands will not be executed until the message is closed. I saw in a question on the forum that there used to be a HSDC Pro v5.201 version that had the option to disable the pop-up messages. Is it still possible to get this version?
3) We thought of trying to write the control software ourselves, is there low-level documentation? For example, how is the capture command carried out, or which address in DDR should be accessed to receive the sampled information?
Thanks a lot
Moshe Oziel