Other Parts Discussed in Thread: ADS54J64EVM, ADS54J64
My goal is to connect the ADS54J64EVM card to a ZC706 via the FMC and use the ADS54J64 in Mode 0, 1, or 6 (LMFS = 4841). I want to start in Mode 0 to get things working, using a Fs = 280MHz. The TI204c IP User guide does not really provide clear instructions on how to build your own project using the TI204C-IP without using the reference design. Does someone have an example Vivado Block Diagram on how this can be implemented or advice on where to start? The user guide keeps noting that the transceiver IP “must be generated using the Vivado Transceiver Wizard” but the reference design does not have you do anything with the wizard so is this an automatic in the reference design?