Part Number: ADS131M08
Other Parts Discussed in Thread: ADS131M06
Dear Colleagues,
this is not a real question, just my experience.
Due to providing the proper common mode voltages to the inputs, I need the half of the reference voltage.
I've thought I can use the REFIN pin as reference output, divide it to half by a resistive divider and then buffer it by an opamp (MCP6V81T) for all other purposes.
I was wrong. This pin cannot tolerate any load. By the way, this is not mentioned in the datasheet, or I just cannot find it.
At the begin, I loaded it with a 2 * 24k resistive divider, and this load was so high ( 50 uA ), that the reference voltage has fallen down to about 50%, 0,6V.
OK, I changed the resistors to 2 * 1MOhm. Now, the reference is 1.1596V, while when completely unloaded (well, 10MOhm by the meter) it is 1.1831V.
This chip is still "virgin", has never seen even a clock signal, nor config data. Power supply is OK, 3.3V each, analog and digital too.
It is hard to imagine, how such a weak reference is able to supply the internal circuitry.
I think, in the next version of the circuit I will use an external reference.