Part Number: AFE4403EVM
Other Parts Discussed in Thread: AFE4403, , AFE4400, AFE4490
Is there any sample or tutorial for the beginners to use AFE4403 EVM GUI and using the data for python or Matlab coding?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AFE4403EVM
Other Parts Discussed in Thread: AFE4403, , AFE4400, AFE4490
Is there any sample or tutorial for the beginners to use AFE4403 EVM GUI and using the data for python or Matlab coding?
Hello Mohammed,
Welcome to the E2E forums!
The AFE4403EVM has a user guide that goes over everything you need to get the EVM up and running. It can be found in the "Technical Documentation" section of the AFE4403EVM page, or visit this link here: https://www.ti.com/lit/pdf/slau572
Kind regards,
Nick Z
Hi Nick,
thank you so much for the information.
please let me know, can the arduino library for AFE4400 or AFE4490 can be used for AFE 4403 for the SPI communication between Arduino uno and AFE4403?
and one more thing, Is there any way to just power up the AFE4403 chip on EVM board and not the MCU of of AFE4403 EVM?
the reason is that I just want to use the AFE4403 chip for the SPI communication with arduino directly and don't want to use the internal MCU of EVM.
Hi,
Not knowing how exactly the pins and the communication protocol you will be using, but you may please take a look of EVM user guide -
5.3 Accessing AFE4403 Digital Signals
and
Figure 85. AFE4403EVM Schematics (1 of 4)

Figure 86. AFE4403EVM Schematics (2 of 4)

to remove the resistors associated with the digital communication pins to AFE. And, customer need to use jumper wires to connect between customer's MCU pins and the nodes/pads that are common/connected to the AFE's digital communication pins(i.e. the resistors sites removed).
Thanks
Hi Yang,
So it seems that I have to remove the resistors.
Please let me know, Will I be able to reconfigure the TIA gain and LED currents (after removing the resistors) by external MCU borad coding?
And one of my previous question is still un-answered that "can the arduino library for AFE4400 or AFE4490 can be used for AFE 4403 for the SPI communication between Arduino uno and AFE4403"?
Hi,
May I ask whether you already used the EVM with GUI to understand the AFE and EVM sufficiently to do some of your evaluation or tests?
If you have and will have only one EVM, it's suggested to do and get familiar with above first before moving on to other external system or master/host.
LED current range and drive current and TIA gain resisters are configurable/set by writing values into the AFE registers.
Please check your arduino board and library and refer to the AFE4403 datasheet section 7.1~7.3, 7.6 and 7.7, if those requirement can be met, then the arduino should be able to work with the AFE4403.
Hi Yang,
Yes, I am evaluating the EVM and after that I will go to for the external MCU.
In my GUI version 2.2, I am have this error when I tried to Launch Macro window from Script option.
In the other red block, the filter option in missing. Is this okay?
Hi,
Could you take a look and follow this thread and to see if this solves the issue?
Thanks
Hi,
Since I did not hear back from you, I believe my suggestions answered your questions.
I will close this post and if you have any pending questions, feel free to post them here or open a new thread.
Thanks and have a great day!