Hello,
I have two questions that contribute to the same phenomenon.
1.The manual states that turning on DLL PDN when Fs is less than 40M can improve the SNR, but when I turn it on, the baseline of data collection will change every time I restart it, and the change range is several mv or even tens of mv. This phenomenon does not occur when the DLL PDN is not enabled.

2.Another problem is when I change the sample rate by changing the mclk frequency, the baseline also changes, which doesn't happen when the mclk frequency doesn't change.
What are the possible causes of the above problems?
Regards