This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
As I am designing High Voltage DC-Link measurement, I have not enough pulse generator for AMC3336.
So, I want to use external pulse oscillator generator at 20MHz to supply CLKIN of AMC3336.
After that, I wan to tuse SDFM (eCAP_CH-04) to measure this voltage.
Would it be applicable for such circuit design ?
And I read that AMC3336 will output 128-bit stream at 10% duty when -1V and 90% duty at +1V.
In such above case, Will SDFM module can work with prior knowing the CLKIN 20Mhz but not knowing the begining of measurement bit ?
Best regards,
Narudol T.
Hi Narudol,
The AMC3336 will output a continuous 1's and 0's density bit stream dependent on the input voltage. The number of bits that are collected for each measurement would depend on the SDFM settings, it is not limited to 128 from the AMC3336 perspective. Using an external 20MHz oscillator is perfectly acceptable and as the bit stream is continuous, the only downside of not knowing when the beginning measurement bit is transferred is that it will take a full cycle of data through the filter before the measurement data is valid.
Please let me know if this makes sense from the AMC3336 perspective or if you have additional questions. If not, I can move this thread as the TMS320F28377D is supported by another group.
Thank you for your answer, yes, the down-side of not knowing the begging of data is what concerning me.
Because I am not familiar with SDFM module. I will check this topic with C2000 forum again.