Part Number: DAC39J84EVM
Other Parts Discussed in Thread: ADC12DJ3200, , ADC12DJ3200EVM
Hi All,
Happy new year to all and hope you are doing great.I working with DAC39J84EVM for an experiment and while connecting DAC to an oscilloscope and ADC for monitoring its response, I am getting dodgy response from the DAC even when no signal is sent through the DAC. The screenshot for the frequency spectrum received on the ADC is attached with the message (similar readings were observed on oscilloscope) (fig. 1). I also tried to send in a sinusoidal pulse centred at 100 MHz from the DAC, the settings of the DAC used and the screenshot for sinusoidal pulse are attached below (fig. 2 and 3). The response received on ADC12DJ3200 is attached as well (fig. 4 and 5). Is it possible to ascertain any reason for such response from the screenshots attached or has the DAC gone completely awry and need to be replaced?
Thanks for your consideration and waiting for your response.