Part Number: ADS4449
The attachment in the related thread has two charts, with digital functions enabled and disabled. Both charts are identical. Is that correct?
If only one or two channels are being used, and the unused channels are not terminated, will that cause high-bit toggles on all channels or just the unterminated channels?
Can this be mitigated by powering down the unterminated channels and/or setting the test pattern to all zeros (or custom pattern for mid-scale)?
e.g. if there is a large deployment in remote locations with unterminated channels, can the problem be mitigated by effectively "disabling" those unused channels in software somehow (to avoid the bit toggles on the used channels).
Thanks, Brendan.