Part Number: DAC8820
Other Parts Discussed in Thread: TIPD194
[1]
Do we have any characterization showing the digital/reference current consumption transients during an output code change/update?
[2]
The datasheet has Figure 7.
It seems like this graph shows the input current (Idd) per digital pin, given the instantaneous input voltage at the pin vs VDD.
Am I understanding it correctly?
[3]
If we don't have data for [1] then could you use the graph in [2] (Figure 7), assuming it was showing input current per digital pin,
to calculate the total input current based on how many input bits were changing state?
Also, does this graph work both ways?
That is, a rising edge from 0V to Vdd on the input shows this trend line, but do we track this trend line on a falling edge as well?
Or am I totally off?