Hi everyone.
I'd like to know if it's possible to make the ADC configuration parameters permanent, i.e., to be persistent on power loss. Every time the 5V power supply to the ADC is interrupted, I have to manually reload the configuration file so the correct sampling rate etc are set for the target application. Is there a flashable memory or something similar to the ADS54J60EVM board that could support that?
Furthermore, I'd like to know if it would be possible to eliminate the usage of the ADS54J60EVM GUI completely. How could I do that? There is no direct SPI header on the device. The option to remove U7 is not viable. Is there any other (more recent) alternative solution? Does a development (non-evaluation) board of this Texas ADC exist in your portfolio?
Kind regards,
Xynos Anastasios