Other Parts Discussed in Thread: ADS1299
Hi,
I have a conceptual doubt regarding the EEG circuit .
I have made circuit using ADS1299, same as given in datasheet Figure 73. I have made BIASREF_INT to (AVSS+AVDD)/2 and connected all BIASP, BIASN open. I am using SRB1 as the reference electrode for all channel. BIAS circuit was enabled with Rf=1Meg Ohm and Rp=47k ohm.
The thing I noticed is that when all channels are kept open in air, touching one channel is showing noise in all channels (with the touched channel having maximum noise). Shouldn't it be like the one which is touched should have noise rest other remain unaffected.
To be sure if one channel introducing noise to all, I shorted channel 2 to 8 with SRB1 and BIAS which was again shorted with circuit ground 0V. Now only channel 1 IN1P is open in air. This time I can only see noise in channel 1 and rest other channel were close to 0V with negligible noise as compared to channel 1.
So overall, why noise in any one channel in air causing noise in other channels too when all channel in air, but not when other channels shorted to some voltage.
Thanks