Hello,
I am using the DAC53004 to control the current in a load with a force-sense configuration with a MOSFET:
We are doing pulses of 50us/250us, with about 20ms rest in-between. Once the pulse is done, we set the DAC-X-DATA registers to 0 and we cut the 9V (so Vd = 0V).
It means that when we cut the 9V, the FB0 sees 0V. At this moment, I can observe a ramp down on the OUT signal. I couldn't find in the datasheet any explanation for this behaviour. I was expecting it to go down to 0V faster. This is what I am seeing: Blue is FB0 and Green is OUT0.
Do you have an explanation for that? is there a way to make the OUT0 go to 0V quicker?
Best Regards,
Aurélie