Dear community and support team,
We have a problem with the ADS131M08. In a current batch we noticed an unusual noise in the output signal of some channels. We then examined this very closely and came to the conclusion that bits are flipping on some channels. According to our measurements, it seems that the first bit of a byte seems to randomly topple, i.e. bit 15 and bit 23. We have not yet ruled out that it also affects bit 7, but this seems to be negligible due to the noisefloor.
For example, we have observed that during a measurement, channels CH1 to CH5 run correctly, and at CH0 the output value jumps and bit 15 flips randomly:
From: 1111 1111 1111 1011 0011 0010 0010 1010.
To: 1111 1111 1011 1011 0010 0101 0011
This gives a jump in the output value from -314838 to -282029. We have documented this in image "ADS131_Failure_CH0.png".

In another measurement, bit 23 at CH5 of the same IC flipped as well.
From: 0000 0111 1000 0110 1010 1111
To: 1000 0111 1000 0110 1100 1101
Which means a significant jump in the output value from 493231 to -7895347. We have documented this in image "ADS131_Failure_CH5.png".

Further measurements show that bits are tilting in certain areas. This could also explain why some channels show no bit errors (jump at the output value) while others have them frequently.
For this we made a measurement and swept the input signal from +0.6V to -0.6V. At first glance you can see almost no error, but if you calculate y(n) = y(n)-y(n-1) you can see very clearly that there are areas where bits flip. Here in this case bit 15 is tilted again. We have attached an image that documents that behavior: "ADS131_Failure_Sweep.png".


As additional infomation, we use the internal reference of the ADS131.
What can cause or explain such a tilting of a bit at the beginning of a byte?
Has such an error or a similar error already been noticed and is there an errata available?
So far, we have only one system where this error occurs. But honestly, we don't know yet how many other systems and ADS131 could be affected.
We therefore ask for a lively discussion here and hope for support on this topic.
Best Regards,
Robert