Other Parts Discussed in Thread: LMK04828
The ADC12DJ3200EVM manual mentions:
The ADC12DJxx00EVM includes a reference clock input (CLKIN0) which allows the user to sync the LMK04828 to an external 10-MHz reference allowing for coherent sampling
It is not clear if any modification to the EVM hardware or software configuration is needed.
My expectation is that applying such 10MHz would improve frequency accuracy of the clock going into the ADC.