Part Number: DDC114
Hello,
My customer tested the DDC114's test mode operation, but it only outputs all F value, not the expected 0 output.
The captured images of the PINs they measured are shown below.
ddc114_interface_waveforms.pdf
1. TEST PIN (PIN31) is HIGH.
2. Same symptom in RANGE 0 to 7.
3. FORMAT PIN (PIN4) is LOW, other pins related to power are normal
Please advise on the cause and solution of TEST mode malfunction.
Thank you.
JH