Other Parts Discussed in Thread: AFE7070
We are using the AFE7070EVM standalone (no TSW1400).
The mixer/NCO is enabled and GUI settings are as shown below. The CMCD7005 is in default state = bypass mode.
LO Input = 2.2 GHz. from signal generator
EXT VCXO Input (J4) = 65 MHz 0 dBm from signal generator
This produces an output spectrum like this which appears to be a lower sideband tone offset by the NCO frequency setting value (1 MHz):
Enabling QMC offset and manually playing with the QMC A & B Offsets the carrier can be nulled = good.

Questions:
1) What is the proper GUI lower left "Clock Settings" when using the EVM this way? It is currently set to single differential SDR clock and with the NCO Fdac setting matching the VCXO input frequency, the output tone is 1 MHz away from the carrier, which matches the GUI NCO Frequency setting. What is Clock settings changing and/or what is the relationship between clock settings and the transmitted result?
2) Enabling QMC Correction and playing with the QMC gain so far only produces worse rejection of the upper sideband. How should adjustments be made to optimize this? Or in other words, what is the procedure to set up an optimized single sideband output and an optimized double sideband output?
3) Are there any other controls that should be adjusted when using the AFE7070 EVM for basic TX output tests?