Part Number: ADS8568
Other Parts Discussed in Thread: ADS8528
Hi,
My customer wants to know the specific parameters of the ADS8568:
1. The ADS85x8 series is an 8-channel ADC. What does it mean in the specification that the maximum data rate per channel is 510kSPS? According to the specification, the 8 channels are divided into 4 conversion pairs. Before the conversion pairs, they communicate in serial order. I would like to ask whether the parameter 510kSPS refers to the data rate when only one conversion pair is working or four conversion pairs. What is the maximum rate that each channel can achieve when all data is transmitted?

2. My customers do not understand the conversion. From the block diagram, we can see that CH_A0 and CH_A1 are the same conversion pair. Does it mean that the sampling and conversion on the two channels are completely synchronized?

3. Finally, confirm one more point: According to the records in the specification, whether it can be understood that the maximum rate of ADS8568 signal acquisition is 650kSPS, and the maximum transmission rate is 510kSPS?
Thanks, and looking forward for your reply~