Part Number: ADS1218
Hello,
I was interfacing ADS1218 ADC with microcontroller Arduino UNO with SPI clock of 1MHz using oscillator of 4MHz. I was able to get the data when I have applied constant DC signal, varying signal to channel (AIN0,AIN1: differential mode) at different sampling rate (up to 100sps and corresponding decimation ratio). But after 1month I have checked again while applying similar sets of input with same code (first writing to registers and reading the registers and then wait for DRDY ,RDATA command then reading data from ADC), when I am reading the registers settings all 16 registers are reading FF values and further no data is coming. Please suggest me what can be the possible solution.
Thank you
Regards
Sushmita Chaudhary
ADC part no: ADS1218Y/150