Part Number: ADS1274EVM-PDK
I met the similar problem when using ads1274EVM-PDK,
And of course, the USB device was enumenated under NI-VISA USB Devices:
My PC is Windows 10 64 bit.
In C:\Program Files (x86)\ADCPro\drivers directory,
I tried to remove the device driver using "mmb0_driver_install_x64-v2.0.0.0.msi",
then double click "mmb0_driver_install_x64-v2.0.0.0.msi" to re-install, but the device was still enumenated under NI-VISA USB Devices.
For the second time, I remove the device driver again, and found the USB device was enumenated "unknown device" under other device in device manager, which was expected. After that, I tried to install the driver manually with "usbstyx.inf" under C:\Program Files (x86)\ADCPro\drivers\usbstyx
But unfortunatedly, system prompt can not install MMBO(NI-VISA), because Windows cannot find device driver
It seems to me that I cannot change the USB device driver from NI-VISA to USBStyx driver. Even though changed another PC (also Windows 10 64 Bit).
BTW, I also have a quick try to attach -5V supply to EVM board. But have no effect.
Could you please give me some suggestions to work the board? Thanks.