Part Number: AFE5809EVM
Other Parts Discussed in Thread: AFE5908, AFE5809
Hi All,
I have a problem with the AFE5809EVM, the AFE5809EVM is triggered in sync with the TSW1400EVM.
For Ramp tests, the test results are normal. The signal is also normal for sinusoidal test mode, but for demod models
Decimation=4, I think the signal from demod is not normal. My input signal is a 10MHz, 20cycles sine burst signal, the clock signal is using 40MHZ, 3VPP external sinusoidal signal, the problem is that in DEMOD mode, I think the output signal should be a sine wave output, But actually only one signal like a triangle wave, is my understanding problematic?
Can you tell me what the AFE5908 LVDS output signal should look like in the DEMOD model when the input signal is a sinusoidal signal and what the acquired signal looks like?
THX.