Part Number: DAC7568EVM
Other Parts Discussed in Thread: DAC7568
We are demonstrating a DAC using the DAC7568EVM.
The specified voltage is output, but if the update frequency is made faster, the output becomes 0.
Please tell me why the output decreases.
-SCLK clock 40MHz ・LDAC pin (DAC7568 1pin) is unused.
-Following the reset command after startup, internal reference power ON is issued.
- Ports A to G and H (SW LDAC at this timing) are updated by polling.
- Output when the polling cycle is 50us. - If the polling cycle is 25us, the output will drop to 0 level.
-The attached data 001_25usCycle-50usCycle CH1#SCLK CH3#OUT-C.jpg / 002_50usCycle-25usCycle CH1#SCLK CH3#OUT-C.jpg is the waveform at that time.
-The same serial data is sent for both polling cycles of 25us and 50us.