Hello,
I asked similar question couple months ago regarding unknown offset in the measurements. The issue has been resolved by running custom calibration, since the offset was uniform at multiple temperature points. Now I'm having an issue with some noise in the measurements.
The RTD setup is as follows,
- IDAC1 and IDAC2 are setup with 500uA
- AIN7 connects positive lead of RTD, AIN6 connect negative lead of RTD
- AIN5 and AIN 4 are selected as external reference
- Reference resistor is 2000K ohm
- ADC2 data rate is selected as 10SPS, PGA = 1
- PT100 RTD is used to measure the temperature, the conversion factor is 0.385Ω/°C. Using the pk to pk noise provided by the data sheet (32.6uV), I was expecting around 0.1693°C noise; 0.385Ω/°C * 500uA = 192.5uV/°C and 32.6uV/192.5uV/°C = around 0.1693°C
The noise I'm seeing is around 0.8°C = around 154uV.
There are few components that I am suspecting as a source of noise but before dive into troubleshooting, I'd like to clarify some questions I have regarding the data sheet.
- The IDAC error spec on page 8 defines the accuracy of the IDAC not the noise
- ex) absolute error of +/-%0.7 means the current output will be within the error
Thanks,
Steven