Part Number: ADS1263
Other Parts Discussed in Thread: ADS1262, , LM2902
Hello,
I'm currently troubleshooting the our ADC circuit to find the source of noise in the signal chain. I've collected 10000 samples at 0.3108V using different data rate and ADCs. I understand the way I measured noise is not how the noise were measured in the datasheet, so it cannot be an exact comparison. However I used the noise performance spec as a reference point as what it can achieve in the right condition. The following lists are the result of collected samples. I've calculated the 6 to compare with the peak-to-peak noise.
Input settings are the same: AINN is tied to AINCOM which is tied to REFOUT. AINP = AIN0. Internal reference is used.
- ADC1 SPS38400 PGA 1
- 6 is around 0.020V
- ADC2 SPS 800 PGA 1
- 6 is around 0.010V
- ADC1 SPS20 PGA 1
- 6 is around 480uV
- ADC2 SPS10 PGA 1
- 6 is around 500uV
Our signal chains involve a lot of different components such as an amplifiers, a multiplexer and opto-isolator. While I'm calculating and measuring noise from other sources, I'd like to ask few questions regarding data sheet.
- Does the internal reference has a noise spec?
- Does PSRR represents the rejection ratio of the power supplied to the ADC?
I think the peak to peak noises are way to big to consider the ADC as a source, but I wanted to know how much internal reference and power supply could contribute to the noise.
I'm attaching a part of ADC schematic here for your reference.

By the way, I'm using the precision noise analysis note. I wanted to say this guided me where to start the troubleshoot :)
Thanks,
Steven