Other Parts Discussed in Thread: DAC8742H
Hi,
I have connected the HART module to the evaluation board In loop-powered. How to check whether the HART module is detected or not? Please let me know if any commands check the detection.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have connected the HART module to the evaluation board In loop-powered. How to check whether the HART module is detected or not? Please let me know if any commands check the detection.
Naresh,
How do you have the DAC8742EVM set up? I assume that you have the input coming in through J7 on the board. If a HART sinusoid appears on the line, the CD pin should go high to indicate the carrier is detected. You should also see the UART signal appear as a result. With an oscilloscope, it would look a little like this:
Note that the DAC8742H uses a 16-byte FIFO buffer, so there is a limit to how much data that can be read at a time. In general, you won't be able to read an entire HART command because of the length of the message.
Joseph Wu