Part Number: ADC121C021
I use two ADC121C021 for sensing temperature.
When I only connected pull down resistor to VIN of the chip, I2C communication is not problem. I2C operate normal.
However, when I connect temperature sensor and read the ADC, there is noise on SDA line and SDA signal not rising at STOP step.
In other words, when a certain voltage level enters the VIN, a problem occurs in the SDA signal.
1) VIN connect GND through resistor(1Kohm) : normal operation

2) noise and not rise SDA signal at STOP step.

3) there is noise on SDA signal, only VIN connect VA through 10Kohm