Hello. I have an inquiry regarding ADS131M08.
I drew the circuit as shown in the photo below, but there is no part related to Single-End in the data sheet, so I would like to inquire whether if the circuit is implemented as above, it will be composed of Single-End 16Ch / Differential 8Ch.

The specifications the customer wants are in the range of Vref -1 to 1, so I think ASD131M08 would be perfect, but I don't understand the Single-End part well, so I'm asking for help.