Part Number: ADC128S052-Q1
Other Parts Discussed in Thread: REF3440,
In the datasheet, current consumption is only given in sum (I(VA) + I(VD)). For my application, I need the maximum current consumption of the analog path at 4.1 V supply (VA, Pin 2). I am sourcing this voltage by a REF3440 that can deliver 10 mA maximum at 4.096 V output.
Assuming maximum 2.6 mA current consumption from the ADC128S052-Q1 (the only information in the datasheet), I would exceed this 10 mA rating by 1.4 mA because of external circuitry that is also supplied by this reference voltage. Reading from the datasheet that the maximum current is voltage dependent and the fact that the digital voltage is supplied separately, I have reason to think that I do not really have a problem. Can you give me a specification that helps me answering that question?
best regards
Martin Maier