Part Number: DAC37J82
Other Parts Discussed in Thread: LMK04828
Hi Ti
I have a question on the Common- and differential mode input level on the DAC37J82
The datasheet states
- Vcom = 0.5V
- Vidpp = 400 to 800 mVp2p
The DAC SYSREF termination on the EVM Board is
- 200 Ohm to ground
- 100 Ohm series + 100 Ohm parallel (voltage divider)
The IBIS model simulation of this setup provides a 200 mV Diff p2psignal with the P&N level at 850 & 1005 mV,
This violated both the Vcom and minimum input Diff voltage specification of the datasheet.
Questions
- What is the minimum Diif input voltage for SYSREF
- Is a Vcom of 1V +/- 200 mV acceptable
Should the DC coupled SYSREF termination be changed to more closely match the SYSREF specification in the datasheet?
Please advise
Thanks
Piet