Hi Team,
Could you please help provide a step-by-step guideline that can help customer understand how to do calibration using register 0x08, 0x09 and 0x0A of this device?
Thanks!
Roy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Roy,
I would recommend doing the following:
As an example, let's say we are in the 0 - 24 mA output range. 1 LSB size is 0.3662 uA. The ideal values at 0x1000 and 0xE000 are 1.5 mA and 22.5 mA.
Let's use measured values of 1.45 mA and 22.3 mA. We need to offset it by 0.05 mA. Dividing this by the LSB gives about 136 LSB, so we can write 0x0088 to the OFFSET Register.
Our new offset measured values are 1.5 mA and 22.35 mA. Dividing the ideal value by our measured value can give us an estimated gain. 22.5 / 22.35 = 1.0067.
Every LSB in the GAIN register is about 0.00001526, centered around x1 at 0x8000. This gives a GAIN register value of 0x81B7.
Let me know if there are any other questions or if I need to clarify more!
Thanks,
Lucas
Hi Lucas,
Thanks for your suggest.
Add more questions :
1. Is there a sequence for zero and span calibration? Will there be any impact?
2. So if we only calibrate Span (not calibrate Zero) and only calibrate the middle value and Span, is it possible that the chip can achieve the ten-thousandth specification?
BR,
Kai
Hi Kai,
1. There isn't really calibration for zero code error, other than using a negaitve VNEG supply and/or using a bipolar output range, if that is what you are asking.
2. Can you elaborate on what you mean by calibrating Span?
Thanks,
Lucas
Hi Lucas,
Thanks for your reply !
So there is no sequence require for zero and span calibration, right?
2. Can you elaborate on what you mean by calibrating Span?
About this question :
2. So if we only calibrate Span (not calibrate Zero) and only calibrate the middle value and Span, is it possible that the chip can achieve the ten-thousandth specification?
is mean achieve the ten-thousandth specification --> 14bit signal range ---> 16384 LSB level can be detect ? They want no matter positive or negative, both have >10000 LSB, is this achievable ?
Add some questions :
1. For example, when calibrating 0-10V and calibrating 5-10V, will the slope obtained be different when applied to the DAC8775?
2. Can the same slope be applied to Bipolar? Or do the positive and negative values need to be calibrated separately?
3. Assume that in Bipolar, only -10V and 10V are calibrated, or only 5V and 10V are calibrated, and a red line is obtained. If this slope is used to fit the DAC8775, will there be any problem with 0V?

BR,
Kai
Hi Paul, Lucas,
Understand, once you back to office, can you help feedback to me ASAP? Thanks!
Kai
Hi Team,
Besides the above questions. Update some issue we are debugging now.
Let me sort out the problems we encountered here.
Customer produced 120pcs, and 20pcs failed with the 0.01% correction.
When initial power on output 0V without correction.
Normal board: output about 0.2~0.4mV
Abnormal board: output 75mV
Their FW team has made several modifications
1. The machine needs to be heated for 30 minutes.
2. Originally, FW only calibrated Span, now theyadded a zero correction mechanism, but since the correction of 0V would not be effective, so the zero correction was changed to a correction of 75mV, and then use mathematical operations to find the zero point.
3. Although this method can be calibrated, the entire production time becomes very long and the production cost increases a lot.
That’s why customer asked us the question in above.
In addition, the normal Zero code Error deviation of TI DAC8775 is plus or minus 2.5mV. Why some of these chip have a deviation of 75mV at initial power on ?

In addition, the part that needs to warm and waite 30 minutes is also strange.
The ppm FSR/°C numbers in the Datasheet are very small. Can you help me confirm whether the DAC8775 needs to be warmed up when calibrating?

BR,
Kai
Hi Kai,
Sorry for the delay, and thank you for the additional information. Lucas should be back in office Friday and will be able to review your questions.
Best,
Katlynne Jones
Hi Katlynne,
Understand there is a holiday in US, but it have been wait for almost 2 weeks, is there anyone who can help at the time ?
Customer can't accept such long pending status.
BR,
Kai
Hi Kai,
I apologize for the extended delay.
Since the calibration steps for Offset are based off of LSB size, you will likely have to update your offset and gain calibration values if you are changing the scale.
Can you share the schematic of the abnormal boards that you are observing?
Thank you,
Lucas
Hi Lucas,
Since the calibration steps for Offset are based off of LSB size, you will likely have to update your offset and gain calibration values if you are changing the scale.
Can you update these process into the step what you have provide in the history ?
- Measure the DAC Output at code values a bit away from zero-code and full-scale (ex. 0x1000 and 0xE000)
- Calculate the slope of the measured points
- Compare these values and slope to the ideal/desired values and slope
- Calculate your calibrated GAIN and OFFSET
- Select your channel by writing to 0x03
- Enable Calibration by writing to 0x08
- Calibrate GAIN by writing to 0x09
- Calibrate OFFSET by writing to 0x0A
Here is the schematic attached at here : AMAX-5024.pdf
BR,
Kai
Hi Kai,
Since different output scales use different/additional circuits inside the device, the amount of LSB needed to calibrate may need to be changed.
I would recommend using all of the steps each time you change the scale, for the most accuracy.
I can do a small test on the values I get on my EVM, to see the relationship between different scales' calibration values.
When you mentioned the part needs to be heated for 30 minutes, what is the customer's reasoning for heating? Does it help resolve the 75 mV issue or something else?
I don't see anything immediately with the schematic.
I would verify that when the customer is externally resetting the device at startup, PVDD and DVDD have reached operational voltages.
Thanks,
Lucas
Hi Lucas,
When you mentioned the part needs to be heated for 30 minutes, what is the customer's reasoning for heating? Does it help resolve the 75 mV issue or something else?
The issue board will have 75mV offset at output when the system just power on, after 30min, this offset will close to 0V. That is why customer said he need to pre-heat for 30min.
BRM
Kai
Hi Kai,
Let me doublecheck with another engineer and I will get back to you soon.
Thanks,
Lucas
Hi Lucas,
Thanks!
If you need a chip to do the FA, please let me know, I'm afraid this is a chip quality issue.
Customer produced 120pcs board this time, and 20pcs failed to pass the 0.01% correction.
And they found, when the system just power on.
Normal board: output about 0.2~0.4mV
Abnormal board: output 75mV at initial, then need about 30min to wait it's output close back to 0.2-0.4mV.
Hi Kai,
What DAC output ranges are the customer observing this 75 mV issue? Can they verify that their negative supply and reference voltage are stable/correct during this event?
If this was only tested on one unipolar range, can they check using a bipolar range as well?
If the issue persists, I may ask for an output plot of several points as well.
Thanks,
Lucas