Part Number: ADS1298R
Dear Expert
We are now designing a 12 lead ECG+RESP+anti defibrillation interference product using ADS1298R. Could you please help us check the issue with the principle design.
Is the connection method of the 12 lead ECG correct?
2. Is the RESP connection method correct?
3. If the above two methods are connected correctly, does it mean that one limb lead V6 is missing?
4. What are the good methods to handle the need for anti defibrillation in products?
5. If ADS1298R cannot design a product with 12 lead ECG+RESP function? Please recommend a product that can perform 12 lead ECG+RESP function.
Please reply as soon as possible, thank you.