Part Number: ADS1261EVM
Other Parts Discussed in Thread: ADS1261, ADS124S08EVM
Hi,
I would like to configure this board for 2 wire RTD measurements. The data sheet provides 3 wire schematics. is this configuration ok for 2 wire 
thanks vadim
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1261EVM
Other Parts Discussed in Thread: ADS1261, ADS124S08EVM
Hi,
I would like to configure this board for 2 wire RTD measurements. The data sheet provides 3 wire schematics. is this configuration ok for 2 wire 
thanks vadim
Hi vadim piskun,
I would check the polarity of the REFx signals in the ADS1261 datasheet to make sure you are connecting the reference resistor to the correct pins. You don't show a ground connection in your drawing (assuming you use a low-side reference resistor), so it's not clear which pin is being used for REFP and which is for REFN.
You also don't show a current source connection in your diagram, nor is there a connection between the RTD and the reference resistor
-Bryan
Hi Bryan,
thanks for your support! Figure 1.4
shows two wire connections. I modified schematic accordingly. Do i use correctly IDAC1 and not IDAC2?

thanks vadim
Hi vadim piskun,
It looks like you are trying to setup a high-side reference, similar to the top right image you included (the bottom right shows a low-side reference). In this configuration, AINCOM will be the current source, correct? If so, this should work
However, you still need a connection to ground so the current has a path to flow. Right now there is no path to ground for the current coming out of AINCOM, so neither the RTD nor the reference resistor will be biased
And, since this is a high-side, you need to add a bias resistor to the bottom of the RTD. See section 2.2 in this document for a discussion about why that bias resistor is needed: https://www.ti.com/lit/an/sbaa275a/sbaa275a.pdf?ts=1705101517845
-Bryan
Thanks Bryan!
Is there by any chance s predefined script for RTD measurements?
thanks vadim
Hi vadim piskun,
I believe there are, but I am not able to check at the moment. You would select from the predefined scripts similar to what is done for the ADS124S08EVM.
You can always copy the command flow from the ADS124S08EVM GUI as well
-Bryan