Hi,
I have a few questions about BQ79600:
1. Which transformer you suggest to use for the communication?
2. What is reverse wakeup?
3. To use reverse wakeup i need to supply 12V to BAT or i can use 5V to BAT and INH without 12V at all?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have a few questions about BQ79600:
1. Which transformer you suggest to use for the communication?
2. What is reverse wakeup?
3. To use reverse wakeup i need to supply 12V to BAT or i can use 5V to BAT and INH without 12V at all?
Thank you
Hi Maor,
This looks like a duplicate of this thread: (+) BQ79600-Q1: BQ79600 Questions - Power management forum - Power management - TI E2E support forums. Which looks like we missed you there. I apologize for the lateness on our part. I will mark that thread as closed and point here. Do not reply to that thread. Only reply to this thread.
1. Which transformer you suggest to use for the communication?
For daisy chain communication, we recommended an inductance of 150-600uH.
Some recommended part numbers are: HMU1228NL, HM2147NL and SM91502AL.
2. What is reverse wakeup?
Reverse wake up is a feature created for when the BQ79600 is in SHUTDOWN (lowest power state) but stack devices are in a state that allow them to communicate (such as sleep). When the stack devices transmit to the base (BQ79600-Q1 in this case), the device goes into VALIDATE mode and can drive the INH pin high when appropriate.
You can find more information in the following sections: Section 7.3.4: INH / Reverse Wakeup , 7.3.3.2.2.3 Fault Transmitting (Automatic Host Wakeup/Reverse Wakeup) when BQ79600-Q1 in SHUTDOWN, 7.3.5 Sniff Detector
3. To use reverse wakeup i need to supply 12V to BAT or i can use 5V to BAT and INH without 12V at all?
Our recommended operating conditions for the voltage at BAT has a minimum of 5.5V.
Let me know if any clarifications are needed!
Best Regards,
Anthony Pham
Hi,
Thank you for the answers. About the transformer, what about HR600599F? datasheet attatched
Hi Maor,
The transformer is within the recommended inductance range.
Best Regards,
Anthony Pham