Hi, guys,
just got ADS1263EVM kit, which includes MMB0 board and 1263-based hat
If I give him power - I see 4 LEDs, indicating different powers and 7-segment indicator, slighly lighting in all segments and dot.
If I connect MMB0 board to USB - I see a new "unknown device".
Looks fine.
ADS1263EVM-PDK-GUI, downloaded today for TI site, installs well, including TI drivers. But GUI software can not connect "to PHI". Reboot does not help.
So I have "unknown device" (Both on Win10 and Win7). If I try to update (in Windows Device Manager) its drivers from the driver installation path ("PHI drivers") it can not find drivers. If I try to reinstall drivers running driver installer - it can not find the device. Looks like the MMB0 board and the driver does not fit each other. The driver install log is attached.
Anybody can help with the problem? (Basic power off/on, reboot, reinstall does not help).