This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1263EVM-PDK: ADS1263EVM

Part Number: ADS1263EVM-PDK
Other Parts Discussed in Thread: ADCPRO

Dear sir,

This week I got the ADS126EVM-PDK evaluation module with MMB0 board. I am working on desktop PC under Window 7 professional OS installed. After the software installation, I clicked EVM and select the ADS126XEVM.

Then after some processing I saw a massage “DSP not ready Retrying…”. After that massage  I saw also “The firmware load has failed due to timeout condition. Please reset the H/W to continue loading the firmware” Pop-up. In this step, I also saw a “e” on display on the MMB0 board.

I am sure all jumper on both board are properly set and the voltages 4 green LED were OK(Green color lights ON).

After that did not process on the ADCPro screen anymore. I have retest it several times but have no change.

Please help me, I attached the captured ADCPro screen.

Best Regards,

6283.status view.pdf