This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1263: can not read data via SPI using STM32 controller

Part Number: ADS1263
Other Parts Discussed in Thread: ADCPRO

Hi,

    as usual - the new ADC - the new connectivity issues.
    So, I have STM32F427 controller and I want to get data from ADC ADS1263 via SPI5 port .

    I have used ADCPro and able to read ADC data successfully under ADC on PC.
    For STM32 case I decided to use the simplest setup (positive active serial data, data active on falling edge, but 16-bit SPI word):
    (I also checked simple SPI loop-back - shorting MOSI and MISO - this works ok.)
     Write Reset (06h) command to ADC
     Write Read Register #0 (20h 00h)
     read data from register #0 - 16 bit
     Write Start ADC1 conversions (08h)
     all this is rendered on pic #1

     Read Register command (2000h) looks unsuccessful, as I can not see ADC ID from register #0. Ok.     
     
     
     After initialization I try to read data from ADC via writing 16-bit command "Start conversion" 0x0012h. This is rendered on pic #2.
     And further - I'm reading 3 x 16bit words. And I always read 210000h.
     So, as I'm not sure if Read Register command works well, I'm not sure ADC readings are meaningful.
     
     Anyway, previously I was able to use this SPI5 port for 16-bit word exchange, so looks like I do something wrong. Please suggest me where I'm wrong.