Part Number: TX7332
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TX7332
Hi,
The T/R switch turn off will be determined by the delay programmed in the register. The T/R switch on delay is counted either from TR_BF_SYNC edge or the end of pattern depending on the TR_SW_DEL_MODE setting. This will happen on every TR_BF_SYNC. TR_EN can be given as a 200Hz (minimum frequency) signal. If possible, it can be given before every TR_BF_SYNC.
Thanks and Regards
Savyan