Hi TI community
We are using DAC161S997 for 4- 20 mA current transmission.
Below attached is the circuit schematics.
We have a problem with bring up of this circuit, that is, while we writing various hex values to the DACCODE register with SPI, the output loop current is not changing from 4 to 20mA.
We have the following observations.
1.The voltage across the loop resistor (250R) is 0.873 V, which means, the current passing through the resistor is appox.3.49 mA, may be the default value in ERR_LOW register. The loop voltage we have given is 24V.
2.We have tried setting the MASK_LOOP_ERR bit of ERR_CONFIG register by 1,and tried the same, but no change in the observation, if we seep the DACCODE Values, loop current was not changing.(we are measuring the current by reading the voltage across the loop resistance).
What could be the reason? Any suggestion for debugging this issue is appreciated.
Thank you in advance.
Warm regards,
Adarsh.