Refer to "Table 9-18,as marked in the red box, DECIMATION FACTOR=6, 8ADC PER LANE MODE is also supported?
Then, there is no 160X/80X/40X/20X mode similar to that described in AFED8JD48 in the AFE58JD28 data sheet. I don’t know if the internal hardware of the two chips is the same?
If you combine the following two figures to see that the highest ADC sampling rate that 8ADC PER lane MODE can support is 40MHz
However, the data rate below is less than the 6.4Gbps of the chip. Please help explain why it is not supported?
8(AD)*2(I+Q)*16bit*80M*10/8/6 = 4.267Gbps
Thanks!