This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7716: DAC7716

Part Number: DAC7716


Dear Support Team,
  We are facing problem to get voltage output from DAC7716 as we did configuration as
AVDD :- +11V
AVSS :- -11 V
DVDD:- No supply
AGND :- GND
DGND :- GND
+5VD :- +5V
REFA :- INTERNAL 2.5 V
LDAC (J2.17) - HIGH( +5V)
RST (S1.3) :- HIGH
Uni/Bip A(J2.8) - HIGH (+5v).
We are monitoring the voltage at DAC channel 1, address 0101, however channel 1 is not producing any output. Is there any way we could obtain an example of code, a schematic of the connections, or setup instructions? Or any example code in Arduino or Embedded or FPGA.
Thanks and Regards
Gowthami Udayagiri