Part Number: DAC81416EVM
Hi,
As mentioned in my previous question, I verified that all the connections and the REFCOMP pin has a 330pF cap as mentioned in the schematic. At the C104 (REF cap) node voltage, I see a of ~2.5V after enabling the internal reference. Now, all the connections have been verified and they seem right to me.
The strange problem is, my DAC is not turning on. It just shows a current of 0.002 A for 15V and -15 V as Vcc and Vss and does not show anything at the channel outputs. The SPI signals are visible on the oscilloscope. When I try to probe CLK pin with my oscilloscope and also hold the back side of my PCB with a finger (which is directly beneath the diode-capacitor circuit that converts 5 V to 3.3 V to provide as Vio to the DAC), my DAC is switching on, shows a current draw of 0.007 mA and also updated the channels. If I let go of my hand from the PCB or remove the oscilloscope cable from CLK pin, it again stops working. This issue certainly does not feel like a SPI timing issue, rather, a design flaw in my circuit. Please let me know how this can be corrected. I am happy to answer any more questions that you might have regarding this.