Part Number: DAC3174
Other Parts Discussed in Thread: TRF3705,
Hello,
I tried the setup as suggested here (previous question), but I'm not getting no signal at the Output for I/Q at all. I'm measuring only 50mV, which is almost zero, ,but no signal at all so something isn't working right..
I checked all voltages and Data Lines, DACCLK and DATACLK, all there, fine, getting to the chip's pins.
I also turned the 4-Wire interface and got to read config0 and it was just like I wrote it the first time again on the SDO line. So I know at least the DAC chip is working and responding, nothing is shorted. TXENABLE and RESETB are both high and Sleep is low..
Am I missing something here? I'm toggeling SYNC to high exactly with the first line of DATA, so it should work just fine.
Just for test purposes: I generated [-1,1] data as sine/cosine wave, then mapped these to [0,4095] for 12-bit output. These data are then converted to binary and fed to each of the Data Lines, so I should measure a sine/cosine wave at I/Q output.
Do you know what I can do more? Maybe I'm missing some registers? These are the one I'm writing just as before:
Any help would be greatly appricated!! DACCLK and DATACLK are running at 50kHz, same as the update of the Data Lines. I also tried to turn up the DACCLK to 1MHz, 10MHz and 100MHz but vainly. I'm almost out of options at this point, since everything else checks out and all LVDS are arriving to the chip reasonably correct.
Thanks!!