Other Parts Discussed in Thread: AFE7950,
I am using TSW14J58EVM with AFE7950 and would like to record 2Rx channels while transmitting 1Tx channel.
It seems that synchronized operation isn't possible so I would like to find out whether a less demanding setup is possible:
1. The Rx and Tx needn't be synchronized (nevertheless, they should overlap most of the time).
2. SW init ("trigger") - no need for external HW trigger.
3. Tx and Rx would be memory based (I generate the Tx signal and analyze the Rx signals in python).
4. Max Bandwidth
Please provide sample code for the init and execution
Best Regards,
Ram