Hello,
We are trying to implement LMFS: 4-2-1-1 in the JESD IP core reference for the zcu102_8b_10b. We want to know which settings in "jesd_link_params.vh" need to be set for our the number of converters (M) and samples per converter per frame (S) for the RX parameters (we are just using XCVR RX lanes for our ADC).
We see in the "TI_204c_IP_ref.sv" that the parameters for M and S can be set for the TX parameters:
We would like to know if there is a similar setting for RX or if setting the TX in this way accomplishes the same task.
Thanks,
Ryan