Part Number: ADC3541
Other Parts Discussed in Thread: ADC3543
Tool/software:
We are currently experimenting with an ADC3543 on a custom board. We like to use the chip in complex decimation mode with parallel DDR output.
Figure 8-36 of the datasheet gives an example of the output format. According to the figure, D16 (MSB) down to D1 (LSB) are used with 16 bit output. I-samples seem to be present on the rising edge of DCLK, Q-samples on the falling edge.
This example does not really go well together with section 8.3.5.5 (Output Bit Mapper) of the datasheet, as Figure 8-44 (for parallel DDR mode) does not even provide addresses for anything below PIN D9. I see no possibility to configure the output bit mapping for PIN D1, D2, ..., D8. Also, I do not see how the addresses for rising and falling edges match to I and Q samples.
So from what I know now, I see two possible interpretations of the datasheet:
1. It is not possible to re-map bits at all in complex decimation output mode and the outputs are always fixed to D16 ... D1
2. The "parallel SDR" output mapping is used to map bits in complex decimation mode
Could you please elaborate a bit on the output bit mapping in complex decimation mode?
- Is interpretation 1) or 2) correct or maybe neither one?
- Is it possible to use more than 16 bits in complex decimation mode with parallel DDR output mode?
- Are there any additional configuration examples (with register contents) that you could provide for complex demication mode in DDR output mode?
Best regards!