Other Parts Discussed in Thread: ADS1298
Tool/software:
Hello,
I'm using an ADS1298ECGFE-PKD evolution board. when I use the evolution kit with ADS1298 software, I can read device IDs and obtain data. As you can see in the image below,
However, as you can see in the image below, I am unable to read the device ID when I disconnect the MMB0 mother board and connect the Ads1298 to the Arduino Uno.
The jumper and pin settings are as follows:
3.3V to J4.9,
5.5V to J4.10,
GND to J4.6,
CS to J3.7,
SCLK to J3.3,
DIN to J3.11,
DOUT to J3.13,
DRDYD to J3.17,
RESET to J3.8
JP2 = 1-2,
JP20 = 2-3,
JP15 = 1-2,
JP24 = 2-3,
JP18 = 2-3,
JP19 = 1-2,
JP21 = 2-3,
JP22 = 2-3,
JP23 = 1-2.
I have verified the voltage at VCAP1 = 1.16V ,VCAP2 = 2.40V ,VCAP3 = 6.8V and VCAP4 = 0.18V. Is everything in our connections are okay? What actions are required to read the device ID of ads1298?