This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51772: schematic check

Part Number: LM51772


Tool/software:

Hi 

Could you help check the below LM51772 schematic and any need to adjust ,Thanks

lm51772.pdf

USB Power Delivery 4-Switch Buck Boost 65W

VIN 4.5V ~ 36V  

VOUT 5V/3A 、9V/3A、12V/3A、15V/3A、20V/3.25A

pd controller adjusts voltage through I2C

USB Power Delivery 4-Switch Buck Boost 20W

VIN 4.5V ~ 36V  

VOUT 5V/3A 、9V/2.3A

pd controller adjusts voltage through I2C