Part Number: DAC39RF10EVM
Other Parts Discussed in Thread: LMX1204
Tool/software:
Hi TI,
I am using DAC39RF10EVM and HSDC Pro to generate single-tone signals (DEM/Dither are both enabled), the sampling rate fs is 1GHz, the input frequency fin can range from 0 to fs/2.
But I found some unexpected spurs on specific frequencies, they are usually equal-spaced in the output spectrum, like when I set fin = 60MHz and 70MHz, the output spectrum is:



But when I set other input frequencies like fin = 110MHz, 160MHz, there are no such spurs :


I want to know what is the cause of these spurs, and is there any suggestion on how to solve them? I also found similar questions in the forum, but it didn't say where the spurs came from: DAC38J84: spurs issues - Data converters forum - Data converters - TI E2E support forums.
Below is my DAC39RF10EVM GUI configuration:
Thanks, looking forward to your reply.